Operator GPO

Operator Library: Hardware Platform

The GPO operator provides an interface to the digital outputs. Via the Pin_ID / PinID parameter (the name of the parameter depends on the hardware platform), you select the digital output (which is wired to a physical pin on a GPIO unit) you want to use for sending a signal.

For all platforms except the imaFlex platforms: If you use a frame grabber with two GPIO units, use the ConnectorType parameter to select the GPIO unit you want to address (GPIO or Front GPIO). On the imaFlex 2 Dual 100, imaFlex CXP-12 Quad and imaFlex CXP-12 Penta platforms, the ConnectorType parameter is not available.

Each digital output can only be used once. Thus, the selected digital output is to be used by exclusively one instance of the GPO operator.

[Note] Front GPO Port Groups on the imaFlex 2 Dual 100 Platform

The front GPO ports on the imaFlex 2 Dual 100 platform are divided into two independent groups:

  • Each group can use a different power supply voltage.

  • GPO and GPI groups do not share the same supply voltage.

  • Each group has its own dedicated power supply pins.

For the mapping of digital inputs and pin connectors, see the GPIO Connectors topic of your frame grabber User Manual. For the imaFlex 2 Dual 100 plaform, see GPIO Connectors (CoF Frame Grabbers).

Available for Hardware Platforms
imaFlex 2 Dual 100
imaFlex CXP-12 Penta
imaFlex CXP-12 Quad
mE 5 marathon VCLx
mE 5 marathon VCL
mE 5 marathon VCX-QP
mE 5 marathon VF2
LightBridge VCL
mE 5 ironman VQ8-CXP6D/-CXP6B
mE 5 ironman VD8-PoCL
pixelPlant 100
pixelPlant 200

Resources

The FPGA device resources of this operator are equal to value of the PinID parameter. You can see the FPGA device resources, if you open the FPGA Device Resources dialog from the Analysis menu. The device resources are read-only:

FPGA Device Resources

Figure 435. FPGA Device Resources


For the imaFlex 2 Dual 100 platform, the resource is of type GPO with index 0 to 7 for Front GPIO connector and 8 to 15 – for the Extension GPIO connector.

For each digital output, one device resource of type TriggerOut is used. See Device Resources for a full list of device resources.

I/O Properties

Property Value
Operator Type M
Input Link I, general purpose output signal to be send out of the frame grabber.

Supported Link Format

Link Parameter Input Link I
Bit Width 1
Arithmetic unsigned
Parallelism 1
Kernel Columns 1
Kernel Rows 1
Img Protocol VALT_SIGNAL
Color Format VAF_GRAY
Color Flavor FL_NONE
Max. Img Width any
Max. Img Height any

Parameters

PinID (all imaFlex platforms)
Type static write parameter
Default FrontGpo0
Range

imaFlex 2 Dual 100: {FrontGpo0, FrontGpo1, FrontGpo2, FrontGpo3, FrontGpo4, FrontGpo5, FrontGpo6, FrontGpo7, ExtensionGpo0, ExtensionGpo1, ExtensionGpo2, ExtensionGpo3, ExtensionGpo4, ExtensionGpo5, ExtensionGpo6, ExtensionGpo7}

imaFlex CXP-12 Penta: {FrontGpo0, FrontGpo1, FrontGpo2, FrontGpo3, ExtensionGpo0, ExtensionGpo1, ExtensionGpo2, ExtensionGpo3, ExtensionGpo4, ExtensionGpo5, ExtensionGpo6, ExtensionGpo7}

imaFlex CXP-12 Quad:{FrontGpo0, FrontGpo1, ExtensionGpo0, ExtensionGpo1, ExtensionGpo2, ExtensionGpo3, ExtensionGpo4, ExtensionGpo5, ExtensionGpo6, ExtensionGpo7}

Via the PinID parameter, you define the digital output (which is wired to a physical pin on a GPIO socket) you want to use for sending a signal. The same digital output can be used only once, i.e., by one instance of the GPO operator.

FrontGpoN represents the GPO for the Front GPIO connector.

ExtensionGpoN represents the GPO for Extension GPIO side connector.

For the mapping of digital inputs and pin connectors, see the GPIO Connectors topic of your frame grabber User Manual. For the imaFlex 2 Dual 100 plaform, see GPIO Connectors (CoF Frame Grabbers).

[Note] Pin Mapping for imaFlex 2 Dual 100
Front GPIO Connector of the imaFlex 2 Dual 100

Figure 436. Front GPIO Connector of the imaFlex 2 Dual 100


GPO Operator PinID Front GPIO Connector Pin GPO Group
FrontGpo0 16 03
FrontGpo1 17 03
FrontGpo2 7 03
FrontGpo3 8 03
FrontGpo4 14 47
FrontGpo5 15 47
FrontGpo6 5 47
FrontGpo7 6 47
Extension GPIO Connector of the imaFlex 2 Dual 100

Figure 437. Extension GPIO Connector of the imaFlex 2 Dual 100


GPO Operator PinID Extension GPIO Connector Pin
ExtensionGpo0 1
ExtensionGpo1 3
ExtensionGpo2 5
ExtensionGpo3 7
ExtensionGpo4 17
ExtensionGpo5 19
ExtensionGpo6 21
ExtensionGpo7 23
[Note] Availability

imaFlex 2 Dual 100, imaFlex CXP-12 Quad, and imaFlex CXP-12 Penta

Pin_ID (mE5 platforms, pixelPlant and LightBridge VCL)
Type static write parameter
Default 0
Range [0;7], [0;3] or [0;1]

Via parameter Pin_ID, you define the digital ouput (which is wired to a physical pin on the GPIO or FrontGPIO socket) you want to use for sending a signal. The same digital output can be used only once, i.e., by one instance of the GPO operator.

[0;7] When you address the GPIO on marathon, or if you use a device with only one GPIO unit (ironman, PixelPlant), the value range is 0 - 7.

[0;3] When you address the GPIO on LightBridge, the value range is 0-3.

[0;1] When you address the Front GPIO on marathon or LightBridge, the value range is 0-1.

[Note] Availability

mE5 marathon VCLx, mE5 marathon VCL, mE5 marathon VCX-QP, mE5 marathon VF2, LightBridge VCL, mE5 ironman VQ8-CXP6D/-CXP6B, mE5 ironman VD8-PoCL, pixelPlant 100, pixelPlant 200

ConnectorType (mE5 marathon and LightBridge VCL platforms)
Type static write parameter
Default GPIO
Range {GPIO, FrontGPIO}

Via parameter ConnectorType, you define which GPIO socket (GPIO or Front GPIO) you want to address with the value you enter for parameter Pin_ID.

[Note] Availability

This parameter is only available for platforms that have a Front GPIO:

  • mE5 marathon VCLx

  • mE5 marathon VCL

  • mE5 marathon VCX-QP

  • mE5 marathon VF2

  • LightBridge VCL

Examples of Use

The use of operator GPO is shown in the following examples: